Pneumatic Basics

Pneumatic Basics

Pneumatic systems are easily created from standard components to deliver a dependable compressed air supply and produce economical motion at machinery, equipment and actuators.

Pneumatic systems are commonly used for creating linear and rotational motion in many kinds of machinery and equipment applications. These systems are assembled from a variety of standard components and use compressed air to achieve controlled motion.

There are other motion control options which may be used instead of or in conjunction with pneumatics. Hydraulics is also a fluid power technology, and it uses uncompressible liquids and can achieve greater forces. Electricactuators can provide more accurate control. However, both are more expensive than pneumatics, and require more maintenance.

Pneumatic systems maintain a well-deserved reputation for offering an excellent combination of compact size, good power availability and reliable operation. These systems can be relatively simple and cost-effective to design, install and maintain compared to other options. This article examines some of the fundamentals necessary to create a pneumatic system.

Pneumatic Parts

Any pneumatic system uses one or more of the following elements:pneumatic pipe line machine with solenoid valve and control valve

Air Supply

Air supply systems are generally compressors, which must be sized to supply a cubic feet per minute (CFM) volume sufficient for all the usage points. There are often several compressors in parallel for redundancy, and they may use alternating start schemes to balance the load. Compressed air can also be connected to storage tanks so the compressors cycle on/off less often. Pneumatic control systems typically use operating pressures between 20 to 130 pounds per square inch (psi). Normally the main line is the highest pressure, which is then stepped down progressively as required for control valves and point of use tools.

Air Filters, Dryers, Lubricators and Pressure Regulatorsindustrial air filter and lubricator

These components may be used at a main upstream location and also downstream at usage points, and they are collectively called air preparation or treatment devices. All air preparation devices serve to protect sensitive downstream components. A variety of filters are available to remove dust, dirt, moisture and compressor oil. Dryers are used when needed to lower the dew point. Pressure regulators maintain a consistent downstream pressure so equipment can operate reliably regardless of the upstream pressure. Some downstream equipment, such as high-speed rotating tools, require a small amount of oil in the air which can be provided by lubricators. Multiple functions may be combined into one device such as a filter/regulator/lubricator (FRL).

Tubing, Hoses and Fittings

Main compressed air pressure is usually routed through pipes. Metal tubing can be used on drop points off the main line when strength and rigidity is needed, but if pressure ratings allow, then flexible tubing and hoses can be run to the points of use. Bulkheads can be selected to quickly connect/disconnect multiple tubing points at one time to facilitate maintenance, while manifolds are a convenient way to distribute many tubing connections. Fittings can be classic threaded, or the much more popular one-touch push connect style. However, it is always important to ensure that matching metric or English sizes are chosen.

Control Valves

Pneumatic control valves will be explored in greater depth with another article. There are several types including manual/mechanical, individual electrical solenoid and multiple manifolded. Manual types are used by service personnel, while mechanical types used to sense positions for pneumatic logic on a machine. Electric solenoid valves, whether individual or ganged in manifolds, are most suitable for automatic control.

Flow Controls and Silencers

Flow controls and silencers are accessories for optimizing and improving equipment operation. Flow controls allow the speed of motion to be individually controlled in each direction. Silencers reduce the sound of exhausting air to provide a quieter operating environment.

Cylinders, Slide Tables, Rotary Actuators and Grippersindustrial linear actuator cylinder

All pneumatic actuators convert air pressure into physical motion. These will also be covered in more detail in another article. Most popular are cylinders, slide tables, rotary actuators and clamps/grippers for motion applications, and quarter-turn actuators to control process valves. These devices come in many sizes and shapes and must be carefully coordinated with the mechanical design. Also, these devices, and how often they operate, determine the required supply of compressed air.

Logic Elements

Although it’s possible to pneumatically perform logic, such as AND and NOT, with the proper components, this type of functionality has largely been superseded by PLC and relay-based automation of electrical solenoids. Some recent designs use PC based programming.

Instrumentation

When automating pneumatic systems, instruments are often incorporated into the control system to provide feedback. For instance, pressure switches can ensure that proper air pressure is present, while position sensors can be used to confirm actuator positioning.

Pneumatic Systems

With a basic understanding of the pneumatic components described in this article, users can create an endless variety of manual and automatic pneumatic systems. Detailed calculations are a good idea and often necessary, however using common sense and ensuring that equipment and fitting sizes are matchedmay suffice.

How helpful was this article? Click a star to rate.
[10 votes so far. Average rating of 4]

LEAVE A REPLY

Please enter your comment!
Please enter your name here